Hygienic Design

Advantages of hygienic design:

Hygienic design from AVENTICS – save, clean, efficient
  • Guaranteed food safety
  • Compliance with hygiene standards
  • Increased energy efficiency
  • Simplified cleaning procedures
  • Reduced downtimes

The best possible food safety – with “best-in-class” components

Processing and producing food products requires particular sensitivity. Extreme care is necessary, especially concerning the hygiene of work processes. Accordingly, the laws, directives and standards governing the requirements are very strict with the aim of maximum food safety.

AVENTICS has expertise in designing hygienic devices that ensure that the foodstuffs currently produced are not contaminated, even with adhering food residue or microorganisms.

This means:

  • Avoiding cavities (recesses and dead spaces), gaps, pointed edges
  • No components that contaminants can accumulate in and avoiding areas that cannot be cleaned
  • Easy cleaning and disinfection
  • Using food-safe materials and lubricants
  • Resistance to chemicals

Optimal hygienic design

Compliance with high hygiene requirements extends the devices' service life and reduces maintenance effort considerably. The result: Production costs decline and efficiency increases.

The solutions that AVENTICS offers for pneumatic automation in the food industry are based on the demanding requirements specified by, for example, the organization EHEDG (European Hygienic Engineering and Design Group) in its subgroup Design Principles. Furthermore, the legal provisions of EN 1672-2:2005 and ISO 14159:2002 are implemented as standards.

From compressed air preparation to the actuator – complete pneumatic automation for the food industry. You can find all the products in our product catalog.

To catalog + eShop 

Important organizations – for further information on food safety

The legislation that deals with food safety in production is immense. The specific aspects of individual standards that apply to different applications must be decided on a case-by-case basis. We recommend an assessment by our experts, who deal with these questions every day. We have compiled an overview of key institutions, authorities, and manufacturers, as well as the most informative journals.

European Hygienic Engineering & Design Group - Aventics

European Hygienic Engineering & Design Group

Practical guidance on hygienic engineering aspects of manufacturing safety is provided by EHEDG.

www.ehedg.org

The Public Health and Safety Organization

A non-profit, non-governmental organization for standards development, product certification, etc.

www.nsf.org

3-A Sanitary Standards Incorporated

A non-profit association representing equipment manufacturers, processors, regulatory sanitarians, etc.

www.3-a.org

Further areas of application

Application example: packaging production

Packaging liquid products places maximum demands on cleanliness. For one of our customers, we worked in collaboration to develop an application-specific packaging system that uses environmentally friendly packaging material and includes an automatic filling station: It's easy to set up, requires little maintenance, and can be operated by only one employee.

Engineering Tools
Configurators
Calculators