Cushioning Via App

Laatzen (Germany), 23.04.2018 | Press

Visualization ensures optimized cylinder cushioning

Many customers use the Aventics Cushioning Adjustment Tool (CAT) to simplify cylinder cushioning adjustment. Aventics has now launched a CAT app to help customers better identify when the optimal state has been reached.

Laatzen (Germany), April 23, 2018 – “Cylinders without effective, custom-set cushioning can strain transported workpieces, shorten the service life of all assemblies, and generate damaging vibrations within the entire machine,” explains Norbert Fortmann, Director Engineering R&D Drives at Aventics. Adjustable pneumatic cushioning is the ideal way to ensure optimal results. When adjusting cushioning with the CAT app, a few turns of the screw are all it takes to ideally adjust the cushioning to the workpiece mass and kinematics.

Additional information on your smartphone

The “CAT by AVENTICS” app visualizes information on the piston speed and the cushioning characteristics for the current cylinder cushioning. When the cylinder is correctly configured, an ideal cushioning curve shows a constantly decreasing piston speed once the piston has retracted into the pneumatic cushioning. An excessively steep curve with abrupt stops or vibration in the end position is an indicator of incorrectly set cushioning.

With the CAT and the accompanying app, users can fully benefit from the excellent features of Aventics cylinders in the system, as incorrect settings become a thing of the past. CAT can be used to commission and check Aventics cylinder series PRA, CSL-RD, MNI, ICL, ITS, TRB, and CCL. The tool adds to Aventics' wide range of engineering and assembly tools.

Under the leading theme “Integrated Industry – Connect & Collaborate,” this year’s Hannover Messe from April 23-27, 2018, will focus on the topic of digital transformation of industry. Aventics will showcase current developments in pneumatics at booth C39 in hall 23.

Contact

Mrs. Christiane Bischoff

Content Marketing & PR Manager

+49 511 2136-870

christiane.bischoff@aventics.com

Contact

Mrs. Meike Müller-Wiegand

Public relations

+49 511 2136-862

meike.mueller-wiegand@aventics.com

Press releases

You need more informations for your work as a journalist? Visit our press release overview.

Press releases